hi all
I need to config the kernel but
bitbake -c menuconfig linux-imx NOT work on ubuntu 18.04 for maaxboard yocto zeus branch
I can not find the solution on Internet.
any help?
error:
bitbake -c menuconfig linux-imx
Loading cache: 100% |#####################################################################################################################################################################################################################| Time: 0:00:03
Loaded 4675 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.44.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "maaxboard-ddr4-2g-sdcard"
DISTRO = "fsl-imx-wayland-lite"
DISTRO_VERSION = "5.4-zeus"
TUNE_FEATURES = "aarch64 cortexa53 crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:cba967414370e195d109353e51510bd829aa86c3"
meta-oe
meta-multimedia
meta-python = "HEAD:9e60d30669a2ad0598e9abf0cd15ee06b523986b"
meta-freescale = "HEAD:c2a0d924f6200eea1fb1d1b61e7420ea5da2f8fb"
meta-freescale-3rdparty = "HEAD:dbcc686f52c3c84db8cb86aa8973a4e373651b98"
meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"
meta-maaxboard = "zeus:4acadd49b4458ed8566991fdb37ab932e93c58b4"
meta-bsp
meta-sdk
meta-ml = "HEAD:752a48385974cbc458c1fcc2e0c8c3f47730914c"
meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"
meta-rust = "HEAD:a012a1027defe28495f06ed522a7a82bdd59a610"
meta-gnome
meta-networking
meta-filesystems = "HEAD:9e60d30669a2ad0598e9abf0cd15ee06b523986b"
meta-qt5 = "HEAD:b8bcf8cb576d072f435a0177375e54424f67d1c9"
meta-python2 = "HEAD:231c3d74cfcf734c3415e86ea8dd97f73ddced9d"
Initialising tasks: 100% |################################################################################################################################################################################################################| Time: 0:00:00
Sstate summary: Wanted 0 Found 0 Missed 0 Current 42 (0% match, 100% complete)
NOTE: Executing Tasks
NOTE: Setscene tasks completed
ERROR: linux-imx-5.4-r0 do_menuconfig: Unable to spawn terminal auto: Execution of '/home/rnd2/work/maaxboard/zeus/imx-yocto-bsp/sources/poky/scripts/oe-gnome-terminal-phonehome /tmp/tmpoqxldxta /home/rnd2/work/maaxboard/zeus/imx-yocto-bsp/maaxboard/build/tmp/work/maaxboard_ddr4_2g_sdcard-poky-linux/linux-imx/5.4-r0/temp/run.do_terminal.31258' failed with exit code 1:
# Error constructing proxy for org.gnome.Terminal:/org/gnome/Terminal/Factory0: Error calling StartServiceByName for org.gnome.Terminal: Timeout was reached
ERROR: Logfile of failure stored in: /home/rnd2/work/maaxboard/zeus/imx-yocto-bsp/maaxboard/build/tmp/work/maaxboard_ddr4_2g_sdcard-poky-linux/linux-imx/5.4-r0/temp/log.do_menuconfig.31258
ERROR: Task (/home/rnd2/work/maaxboard/zeus/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb:do_menuconfig) failed with exit code '1'
解決済! 解決策の投稿を見る。
hi @Bio_TICFSL
Thank you
I find a solution from here:
https://unix.stackexchange.com/questions/297362/yocto-bitbake-does-not-start-menuconfig
works now.
My solution was to edit the terminal.py file into the poky directory as :
sources/poky/meta/lib/oe/terminal.py and add the dbus-lanch.
line 56 : command = 'dbus-launch gnome-terminal -t "{title}" --disable-factory -x {command}'
Hello Jin1
Looks like it has some problems with gnome, the i.MX don´t use gnome so I guess this is from your settings. For the issue the gnome address is not available.
Regards
hi @Bio_TICFSL
Thank you
I find a solution from here:
https://unix.stackexchange.com/questions/297362/yocto-bitbake-does-not-start-menuconfig
works now.
My solution was to edit the terminal.py file into the poky directory as :
sources/poky/meta/lib/oe/terminal.py and add the dbus-lanch.
line 56 : command = 'dbus-launch gnome-terminal -t "{title}" --disable-factory -x {command}'