From DDR3 documentation, I understand that there are 4 types of calibrations that can be done. Namely,
Are these supported in the uboot code for iMX6 ? I haven't found any mention of them for the iMX6Q sabresd reference board.
We are designing a new board based on the iMX6D processor using two DDR3 chips from Nanya on a 32-bit bus totally 1GB of RAM. We have used daisy chain topology for our new board and we feel that we may need these calibrations during bringup. Do you have any idea how we can do these?
-Abraham V.
解決済! 解決策の投稿を見る。
Hi, Abraham
The DCD table has done all the calibration you mentioned, see below from flash_header.S, you can get them from MMDC chapter of RM.
/* HW ZQ */
328 MXC_DCD_ITEM(39, MMDC_P0_BASE_ADDR + 0x800, 0xA1390003)
329
/* Write leveling */
330 MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)
331 MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)
332 MXC_DCD_ITEM(42, MMDC_P1_BASE_ADDR + 0x80c, 0x001F001F)
333 MXC_DCD_ITEM(43, MMDC_P1_BASE_ADDR + 0x810, 0x001F001F)
334
335 MXC_DCD_ITEM(44, MMDC_P0_BASE_ADDR + 0x83c, 0x4333033F)
336 MXC_DCD_ITEM(45, MMDC_P0_BASE_ADDR + 0x840, 0x032C031D)
337 MXC_DCD_ITEM(46, MMDC_P1_BASE_ADDR + 0x83c, 0x43200332)
338 MXC_DCD_ITEM(47, MMDC_P1_BASE_ADDR + 0x840, 0x031A026A)
/* Read calibration */
339 MXC_DCD_ITEM(48, MMDC_P0_BASE_ADDR + 0x848, 0x4D464746)
340 MXC_DCD_ITEM(49, MMDC_P1_BASE_ADDR + 0x848, 0x47453F4D)
/* Write calibration */
341 MXC_DCD_ITEM(50, MMDC_P0_BASE_ADDR + 0x850, 0x3E434440)
342 MXC_DCD_ITEM(51, MMDC_P1_BASE_ADDR + 0x850, 0x47384839)
These values which are used to set to the MMDC registers were the results from the calibration.
As I read from posts here, the calibration can't be done in the DCD table, is that right?
I am new to iMx6, and just started working on this, like to confirm my understanding is right.
Thanks.
Best regards.
Kan
Hi, Abraham
The DCD table has done all the calibration you mentioned, see below from flash_header.S, you can get them from MMDC chapter of RM.
/* HW ZQ */
328 MXC_DCD_ITEM(39, MMDC_P0_BASE_ADDR + 0x800, 0xA1390003)
329
/* Write leveling */
330 MXC_DCD_ITEM(40, MMDC_P0_BASE_ADDR + 0x80c, 0x001F001F)
331 MXC_DCD_ITEM(41, MMDC_P0_BASE_ADDR + 0x810, 0x001F001F)
332 MXC_DCD_ITEM(42, MMDC_P1_BASE_ADDR + 0x80c, 0x001F001F)
333 MXC_DCD_ITEM(43, MMDC_P1_BASE_ADDR + 0x810, 0x001F001F)
334
335 MXC_DCD_ITEM(44, MMDC_P0_BASE_ADDR + 0x83c, 0x4333033F)
336 MXC_DCD_ITEM(45, MMDC_P0_BASE_ADDR + 0x840, 0x032C031D)
337 MXC_DCD_ITEM(46, MMDC_P1_BASE_ADDR + 0x83c, 0x43200332)
338 MXC_DCD_ITEM(47, MMDC_P1_BASE_ADDR + 0x840, 0x031A026A)
/* Read calibration */
339 MXC_DCD_ITEM(48, MMDC_P0_BASE_ADDR + 0x848, 0x4D464746)
340 MXC_DCD_ITEM(49, MMDC_P1_BASE_ADDR + 0x848, 0x47453F4D)
/* Write calibration */
341 MXC_DCD_ITEM(50, MMDC_P0_BASE_ADDR + 0x850, 0x3E434440)
342 MXC_DCD_ITEM(51, MMDC_P1_BASE_ADDR + 0x850, 0x47384839)
These values which are used to set to the MMDC registers were the results from the calibration.
As I read from posts here, the calibration can't be done in the DCD table, is that right?
I am new to iMx6, and just started working on this, like to confirm my understanding is right.
Thanks.
Best regards.
Kan
Thank you. Looks like that was what I needed.
I have a supplementary question involving some of those registers. If we look in the iMX6 reference manual the four registers,
MMDC Core ODT Timing Control Register (MMDCx_MDOTC)
MMDC Core Timing Configuration Register 0 (MMDCx_MDCFG0)
MMDC Core Timing Configuration Register 1 (MMDCx_MDCFG1)
MMDC Core Timing Configuration Register 2 (MMDCx_MDCFG2)
define timing parameters for DDR3. It's specified in terms of clocks. (eg: MMDCx_MDCFG0: tRFC bits31-24 can be configured as either 1 clock, 2 clock, ... 256 clocks). Is this referring to the external clock on DDR bus or some internal MMDC clock?
-Abraham V.
Hi, Abraham
This is referring to the external clock of DDR BUS, such as on i.MX6Q, it is 528M.
Thanks!
-Abraham V.
HI, Abraham
You may check the flash_header.S, the DDR3 calibration should be done in DCD table.