about basler in imx8mplus,isp-server failed!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about basler in imx8mplus,isp-server failed!

1,182 Views
lidongxu
Contributor II

Hi NXP~

I want to run the Basler driver on imx8mp EVK recently, so I followed the tutorial in README in the ISP file I downloaded from the NXP official website (LF5.15.52_2.1.0). However, when I ran insmod modules/basler-camera-driver-vvcam.ko is failed, and when I followed the process to the end, the ISP server also failed to start. What is the reason for this?

lidongxu_1-1702267614356.png

 

lidongxu_0-1702267238770.png

lidongxu_2-1702267642731.pnglidongxu_3-1702267656132.png

 

 

Labels (2)
0 Kudos
Reply
1 Reply

1,167 Views
joanxie
NXP TechSupport
NXP TechSupport

which basler do you use? did you change the dtb file to imx8mp-evk-basler.dtb? if yes, the current bsp should already include the modules, you can use lsmod to check it, if you use DAA3840-30MC which is supported by the current bsp as default, after you boot up, you can just use gstreamer to capture video directly

0 Kudos
Reply