Looking into an issue with SPI and are trying to determine if we have an issue inside our mid-level driver, which we suspect, or if something else is going on. I am wondering if you have seen any issues with the SPI on the i.MX6, specifically anything with the slave strobe on read and write. I am looking for errata information or any known issues with the Linux 3.0.35 reference design. I am trying to eliminate anything from the silicon up to our mid-level driver as an issue. Any information you can provide would be helpful.
Hi Scott
there are no silicon issues with i.MX6Q eCSPI, just for reference example
and errata document IMX6DQCE
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------