Reducing standby power consumption of SABRE Lite board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reducing standby power consumption of SABRE Lite board

457 Views
victhorf
Contributor II

I have noticed my SABRE Lite board consumes around 100 mA @ 5V during suspend, with the Ethernet cable unplugged. I'm wondering if it is possible to connect the EN pins of the +2.5V and +1.2V (core voltage) regulators to GPIO pins on the i.MX6 and turn them off during suspend, then turn them back on during resume.

Board schematics: Dropbox - schematic

Labels (1)
0 Kudos
1 Reply

334 Views
igorpadykov
NXP Employee
NXP Employee

Hi Victhor

core voltage can not be disabled, they can be just lowered

(0.9V for VDD_ARM_IN ) during low power modes. One can check

IMX6DQCEC Table 6. Operating Ranges

Table 9. Stop Mode Current and Power Consumption

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos