Why are all Qt windows full screen in i.mx6q Qt 5.xxx ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why are all Qt windows full screen in i.mx6q Qt 5.xxx ?

786件の閲覧回数
bluedrum
Contributor I

I am using Qt5.8 to port a project in imx6q.

Qt 5.8 from NXP yocto .

I found that all windows (such as dialogs, main window) are forced to display full screen.

No matter how you adjust setWindowFlag(), it is always full screen.

The original layout was completely destroyed,

Hard to see the eglfs mode only full screen?

ラベル(4)
0 件の賞賛
返信
1 返信

656件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

one can try with nxp bsps and follow sect.5.6.7 Qt 5 attached Yocto Guide.

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信