Hi Community.
We are developing products using i.MX8M Mini. On our board, we use Lattice's "MIPI D-PHY to CMOS Interface Bridge Soft IP"(http://www.latticesemi.com/view_document?document_id=51675 ) CPLD for MIPI-DSI to LVDS conversion. Parameter setting of CPLD is fixed, and parameter setting by I2C / SPI from CPU is not performed.
I am looking for a simple kernel driver (driver/gpu/drm/panel) only for MIPI-DSI, but I am not sure which one to use.
Which driver is appropriate to use the above Lattice Bridge Soft IP?
Best Regards,
T.Kashiwagi
已解决! 转到解答。
Hi Kashiwagi
one can start with raydium panel driver
panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel
all MIPI DSI drivers are described in sect.Table 6-12. MIPI DSI Driver Files attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kashiwagi
one can start with raydium panel driver
panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel
all MIPI DSI drivers are described in sect.Table 6-12. MIPI DSI Driver Files attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor-san
Thank you for reply.
I think that it can be used except for unnecessary parts such as the reset command. I will create a new driver based on this code.
Best Regards,
T.Kashiwagi
Hello @Takashi_Kashiwagi ,
We are also integrating a MIPI-DSI to LVDS bridge in our design based on a imx8mm. Our bridge is very simple and does not need external configuration.
We are then struggling with the removal of the communication parts. Have you successfully integrated your IP ? if yes, do you have some hints on what should be remove in the raydium rm67191 driver ?
Thank you in advance for your response.
Best regards,
Alexandre Fiset
In our case, we adopted "MIPI-DSI to RGB" conversion due to IP reasons.
> We are then struggling with the removal of the communication parts. Have you successfully integrated > your IP ? if yes, do you have some hints on what should be remove in the raydium rm67191 driver ?
In our case, I didn't use the "raydium rm67191 driver".
We used only one type of display, so I added a new display definition to "panel-simple.c" and a new display using panel-simple to the device tree.
Best Regards,
T.Kashiwagi