Whether the DDR calibration stress tool can support 200MHz?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Whether the DDR calibration stress tool can support 200MHz?

911件の閲覧回数
caritzhu
Contributor III

Our project need to set DDR clock as 200MHz on the iMX6Q board, but I find the DDR calibration stress tool can only support calibration between 300Mhz and 528Mhz. How can I calibrate the DDR parameter under 200Mhz DDR clock?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

783件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  200 MHz is relatively low frequency for DRAM, and calibration is not necessary.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

------------------------------------------------------------------------------

0 件の賞賛
返信

783件の閲覧回数
caritzhu
Contributor III

Thank you for your reply, so I need to turn off the calibration when uboot startup? or just to ignore the DDR calibration parameter.

Thank you

Carit

0 件の賞賛
返信

783件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may find (or test) experimentally calibration parameters, setting manually,
which will be used  in Your boards. 

Regards,

Yuri.

0 件の賞賛
返信