Where is updated documents about 32bit DDR3 Script for 3.10.53 BSP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is updated documents about 32bit DDR3 Script for 3.10.53 BSP?

ソリューションへジャンプ
1,416件の閲覧回数
JHY
Contributor IV

I have read below link but can not find board/freescale/mx6q_sabresd/flash_header.S.

Futhermore other files in most of documents are not exist, it is concerned with old BSP, I think.

How to Create i.MX6 32bit DDR3 Script Based on 64bit DDR3 Script

Where is updated documents about 32bit DDR3 Script for 3.10.53 BSP?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,053件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

ddr configured in *.cfg files, like uboot../board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg

so one needs to modify it for 32bit memory configuration

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,053件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

32bit memory configuration is supported in FSL 3.10.53 BSP

refer to attached Linux Guide sect.5 "Enabling Solo Emulation"

included in L3.10.53_1.1.0_LINUX_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,053件の閲覧回数
JHY
Contributor IV

It looks like more setting is needed, because it is a guide of u-boot for i.MX 6Solo on an i.MX 6DualLite SABRE-SD and my sabre board has i.MX 6Quad.

What is missing point for i.MX6 Quad system?

0 件の賞賛
返信
1,054件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

ddr configured in *.cfg files, like uboot../board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg

so one needs to modify it for 32bit memory configuration

0 件の賞賛
返信