HI,i am using the imx8mm evk.
When i set the sw1101 1010xxxxxx,sw1102 xxxxxxxxx0,i execute the cmd:
sudo ./uuu_imx_android_flash.sh -f imx8mm -a -e -t sd,the log is as follows:
This script is validated with uuu 1.2.135 version, please align with this version.
dtbo is supported
dual slot is supported
generate lines to flash u-boot-imx8mm.imx to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.135-0-gacaf035
Wait for Known USB Device Appear...
It should cann't find the device?
It can't burn it.
解決済! 解決策の投稿を見る。
>>Can I use this cable to download!
Yes, the cable is correct.
One side is USB TYPE-C, the other side is USB TYPE-A-M.
weidong
Hello Tangyuan,
The issue is very simliar to the descriptions in the document.
So you can refer to it.
https://community.nxp.com/docs/DOC-342719
Have a nice day!
B.R,
Weidong
HI,sun
I found that i power on the board, i can't find the HID compliant device.
Hi tang yuan,
According to schematic, your setting is no problem. But there are 2 USB Type-C connectors on i.MX8M Mini board, J301 and J302, J302 is for power input, J301 is used for download purpose. See test below:
1. connection
2. Connecting it to Windows USB Port
Then begin to install HID driver.
So no problem.
Have a nice day!
B.R,
Weidong
HI,sun
Thank you very much for your answer!
I see the official documents as follows:
It said that the J301 is used for mouse! But i has a blank cable indeed as follows:
Can I use this cable to download!
>>Can I use this cable to download!
Yes, the cable is correct.
One side is USB TYPE-C, the other side is USB TYPE-A-M.
weidong
Thank you ,Sun,
The problem is solved