When the imx8mmevk enter ino the download mode ,it report the error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When the imx8mmevk enter ino the download mode ,it report the error

Jump to solution
2,806 Views
tangyuan
Contributor III

HI,i am using the imx8mm evk.

When i set the sw1101 1010xxxxxx,sw1102 xxxxxxxxx0,i execute the cmd:

 sudo ./uuu_imx_android_flash.sh -f imx8mm -a -e -t sd,the log is as follows:

This script is validated with uuu 1.2.135 version, please align with this version.
dtbo is supported
dual slot is supported
generate lines to flash u-boot-imx8mm.imx to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.135-0-gacaf035

Wait for Known USB Device Appear...

It should cann't find the device?

It can't burn it.

Labels (1)
1 Solution
2,546 Views
weidong_sun
NXP TechSupport
NXP TechSupport

>>Can I use this cable to download!

Yes, the cable is correct.

One side is USB TYPE-C, the other side is USB TYPE-A-M.

weidong

View solution in original post

0 Kudos
Reply
6 Replies
2,546 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Tangyuan,

  The issue is very simliar to the descriptions in the document.

  So you can refer to it.

https://community.nxp.com/docs/DOC-342719 

Have a nice day!

B.R,

Weidong

0 Kudos
Reply
2,546 Views
tangyuan
Contributor III

HI,sun 

     I found that i power on the board, i can't find the HID compliant device.

0 Kudos
Reply
2,546 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi tang yuan,

pastedImage_2.png

According to schematic, your setting is no problem. But there are 2 USB Type-C connectors on i.MX8M Mini board, J301 and J302,  J302 is for power input, J301 is used for download purpose.  See test below:

1. connection

pastedImage_3.png

2. Connecting it to Windows USB Port

pastedImage_4.png

Then begin to install HID driver.

pastedImage_5.png

So no problem.

Have a nice day!

B.R,

Weidong

2,546 Views
tangyuan
Contributor III

HI,sun

      Thank you very much for your answer!

      I see the official documents as follows:

      1111.png

      It said that the J301 is used for mouse! But i has a blank cable indeed as follows:

     2222.jpg

Can I use this cable to download!

0 Kudos
Reply
2,547 Views
weidong_sun
NXP TechSupport
NXP TechSupport

>>Can I use this cable to download!

Yes, the cable is correct.

One side is USB TYPE-C, the other side is USB TYPE-A-M.

weidong

0 Kudos
Reply
2,546 Views
tangyuan
Contributor III

Thank you ,Sun,

 The problem is solved

0 Kudos
Reply