What is the mean of "JPEG_ENC_YUV_FORMAT"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the mean of "JPEG_ENC_YUV_FORMAT"

925 次查看
yongtang
Contributor I

I observed the define of "JPEG_ENC_YUV_FORMAT" in <jpeg_enc_interface.h>,but i could not understand the mean of "NONINTERLEAVED" and "INTERLEAVED",is means "packet" and "plain"? I want use g2d_blit to resize the image and then encode with jpeg,but there have two types of image format define as below,how can i use these?

enum g2d_format

{

//rgb formats

     G2D_RGB565               = 0,

     G2D_RGBA8888             = 1,

     G2D_RGBX8888             = 2,

     G2D_BGRA8888             = 3,

     G2D_BGRX8888             = 4,

     G2D_BGR565               = 5,

     G2D_ARGB8888             = 6,

     G2D_ABGR8888             = 7,

     G2D_XRGB8888             = 8,

     G2D_XBGR8888             = 9,

//yuv formats

     G2D_NV12                 = 20,

     G2D_I420                 = 21,

     G2D_YV12                 = 22,

     G2D_NV21                 = 23,

     G2D_YUYV                 = 24,

     G2D_YVYU                 = 25,

     G2D_UYVY                 = 26,

     G2D_VYUY                 = 27,

     G2D_NV16                 = 28,

     G2D_NV61                 = 29,

};

typedef enum

{

      JPEG_ENC_YUV_444_NONINTERLEAVED,

      JPEG_ENC_YUV_422_NONINTERLEAVED,

      JPEG_ENC_YUV_420_NONINTERLEAVED,

      JPEG_ENC_YU_YV_422_INTERLEAVED,

      JPEG_ENC_YV_YU_422_INTERLEAVED,

      JPEG_ENC_UY_VY_422_INTERLEAVED,

      JPEG_ENC_VY_UY_422_INTERLEAVED

}JPEG_ENC_YUV_FORMAT;

标签 (1)
0 项奖励
回复
2 回复数

784 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yong

for interleaved format usage one can look at IPU, VPU presentations below

and VDOA description in Chapter 68 i.MX6Q Reference Manual

https://community.freescale.com/docs/DOC-95595 p.31

https://community.freescale.com/docs/DOC-100482   p.122

Best regards

igor

0 项奖励
回复

784 次查看
yongtang
Contributor I

And what is the memory layout of "JPEG_ENC_YUV_FORMAT"?

0 项奖励
回复