Hello,
What is the difference between Parameter Register's Frame Size and SAI Transmit Configuration 4 Register 's Frame Size?
Thank you.
已解决! 转到解答。
Hi ma
Parameter Register's (read only) shows sai configuration implemented in that processor:
for example FRAME (Frame Size) =5 : The maximum number of slots per frame is 2^FRAME: 32
This corresponds description for SAI Transmit Configuration 4 Register (TCR4):
"FRSZ -The maximum supported frame size is 32 words."
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ma
Parameter Register's (read only) shows sai configuration implemented in that processor:
for example FRAME (Frame Size) =5 : The maximum number of slots per frame is 2^FRAME: 32
This corresponds description for SAI Transmit Configuration 4 Register (TCR4):
"FRSZ -The maximum supported frame size is 32 words."
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------