Hello,
What is the difference between Parameter Register's Frame Size and SAI Transmit Configuration 4 Register 's Frame Size?
Thank you.
解決済! 解決策の投稿を見る。
Hi ma
Parameter Register's (read only) shows sai configuration implemented in that processor:
for example FRAME (Frame Size) =5 : The maximum number of slots per frame is 2^FRAME: 32
This corresponds description for SAI Transmit Configuration 4 Register (TCR4):
"FRSZ -The maximum supported frame size is 32 words."
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you very much!
Hi,
So Parameter Register's Frame Size is only going to be 5 at most, even if it has 4 bits, right?
Parameter Register shows what max. Frame Size is implemented in
that processor silicon sai module. In other processors silicons it may have other values.
Best regards
igor
Hi ma
Parameter Register's (read only) shows sai configuration implemented in that processor:
for example FRAME (Frame Size) =5 : The maximum number of slots per frame is 2^FRAME: 32
This corresponds description for SAI Transmit Configuration 4 Register (TCR4):
"FRSZ -The maximum supported frame size is 32 words."
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------