What happens for the Yocto Linux rootfs size?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What happens for the Yocto Linux rootfs size?

6,240 Views
13614278
Contributor III

We are using IMX8mini EVK, which is 8G emmc, running Yocto Linux

By default, the bitbake fsl-image-validation-imx would created a 1.3GB size of rootfs, like fsl-image-validation-imx-imx8mmevk.sdcard.bz2

After flashing the whole image, the linux would show the rootfs(/) is the same size as 1.3GB. But we all know our emmc is 8GB.

And I struggling this, found if add IMAGE_ROOTFS_SIZE with large number to increase the whole size. 

Obviouslly, this is un-reasonable, as we have to create 8GB file size of rootfs image, that's too large for both flash and copying. I am really feel confused that why Yocto Linux use such method? As most of the data byte must be ZERO-padding for this case, this is unnecessary at all.

For Android, the whole system.img is just 800MB, but the whole 8GB emmc can be usable and visable.

How could I let Yocto Linux have real data size(e.g, just 400MB), but the whole emmc storage also be visable and usable?

2 Replies

5,998 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yang Songxiang,

I agree that it’s hard to fir the resulting image to your storage size. The following document may be helpful:

https://community.nxp.com/docs/DOC-105521

I would recommend increasing the free space (IMAGE_ROOTFS_EXTRA_SPACE), which is an easier parameter to setup in order to maximize the use of the storage used.

Regards,

5,998 Views
13614278
Contributor III

Thank you very much, this is the first time that I got my expected answer on this website.

0 Kudos
Reply