We need fast boot in my i.MX6 Quad based medical tablet application. Can you tell me if 256MB NOR FLASH (MT25QL02GCBB8E12-0SIT) in QSPI mode is suitable for fast boot? or we have to use NAND flash to achieve Fast Boot in my application?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

We need fast boot in my i.MX6 Quad based medical tablet application. Can you tell me if 256MB NOR FLASH (MT25QL02GCBB8E12-0SIT) in QSPI mode is suitable for fast boot? or we have to use NAND flash to achieve Fast Boot in my application?

751 次查看
sagar_kumar
Contributor I

Hi

We need fast boot in my i.MX6 Quad based medical tablet application. Can you tell me if 256MB NOR FLASH (MT25QL02GCBB8E12-0SIT) in QSPI mode is suitable for fast boot? or we have to use NAND flash to achieve Fast Boot in my application?

Thanks

Sagar

0 项奖励
回复
1 回复

672 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  Fast boot option may be considered from two points of view:

1)  physically fast boot is special eMMC boot mode, supported by i.MX6 boot ROM;

2) general system (Linux) fast boot. 

 

  As for Your system: note, i.MX6 does not support QSPI NOR boot - only SPI (1-bit) may be used.

Also, please refer to https://community.nxp.com/message/1102150 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复