Hi,
We have designed board based on the NXPs i.MX8MQ SoC(Industrial grade), Here we are facing watch dog reset issue.
While running the board or if keep the board in ideal state board is getting reset automatically without any error prints.
When we disable the frequency switching, issue is not there(Fixed to either 800MHz with 0.9V Voltage level or 1.3GHz with 1V Voltage level). When we run the frequency switching only issue is observed.
I have attached the log.
Best regards,
MK
Hi,
Any update on my above issue ?
Best regards,
MK