Wandboard DL SD card readiness

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wandboard DL SD card readiness

940 次查看
lyfsci
Contributor III

Hi Experts,

I am not able to find procedure for flashing the Android 5.0.1 build into the SD card for Wandboard DL. I am able to successfully compile the repository and the images are generated. It would be great if I could be pointed to few documentation regarding the same.

I tried flashing using the fsl script where it expects "u-boot.imx" file which is not generated as part of compilation.

Regards,

Lyf

标签 (3)
0 项奖励
回复
1 回复

862 次查看
art
NXP Employee
NXP Employee

Refer to attached Quick Start Guide document (starting from the Page 2). This document is also available on the Wandboard web site:

http://www.wandboard.org/index.php/downloads


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复