WDOG2 of i.MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WDOG2 of i.MX6DL

756件の閲覧回数
宗標廖
Contributor V

Hello Community

I did following tests on i.MX6DLSabreauto board and i.MX6Sabresd board .

1)test steps

/unit_tests/memtool -16 0x20c0000=0x34

2)result

On sabresd board, after run the command above, the board reboots.

On sabreauto board, after run the command above, the board does not reboot and the following error comes out.

snvs-secvio 20cc000.caam-snvs: Unhandled Security Violation Interrupt 2 = Watchdog

could you tell me why WDOG2 is different on sabreauto board and sabresd board?

Thank you!

ZongbiaoLiao

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

526件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

WDOG2 on sabresd board is connected to PMIC PWRON

and resets PMIC, while on sabreauto board it is not connected in such way.

Error may appear since WDOG2 is dedicated to TZ, description

can be found on sect.70.4 Watchdog mechanism and system integration

i.MX6SDL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

526件の閲覧回数
宗標廖
Contributor V

Hi igor

Thank you for your reply!

Please tell me how to enable WDOG2 on sabreauto board.

Thank you!

ZongbiaoLiao

0 件の賞賛
返信