I updated my BSP recipes from LF5.10.72_2.2.0(Yocto 3.3 hardknott) to LF5.15.32_2.0.0(Yocto 4.0 kirkstone)
My procedure was written in "3 Host Setup" to "5 Image Build" of i.MX Yocto Project User's Guide.
After building, It seems the image file be built but the following WARNING was shown.
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe sigma-dut [license-file-missing]
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe sudo [license-file-missing]
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe sudo [license-file-missing]
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe sudo [license-file-missing]
WARNING: imx-image-full-1.0-r0 do_rootfs: QA Issue: The license listed BSD was not in the licenses collected for recipe wireless-tools [license-file-missing]
May I ignore these WARNINGs?
If not, how should these be resolved?
Best regards.
tanoue.
I think my image's behavior is fine.
However, I worry about these WARNING may have some issue.
For example, if licenses of the recipes are not written in license.manifest in my yocto project.
If it occurs, I can't know all licenses in my product. This is a problem.