VPU Driver Test on WEC7-i.MX6 Platfrom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPU Driver Test on WEC7-i.MX6 Platfrom

1,627 Views
Ashfaque
Contributor II

Hello all,

During testing of the VPU basic driver application  (ENCTEST & DECTEST) provided by the Freescale for i.MX6 processor platform for Windows Embedded Compact 7 (WEC 7) results in VPU encoder failing. 

Below error message was displayed on running the Encoder Test Application. 

PID:00400004 TID:058E013A ERROR: g:\wince700\platform\common\src\soc\mx6q_fsl_v3\vpu\code\vpu_helper.cpp line 458: PID:00400005 TID:058E013A Wrong offset and/or encode size!
PID:00400005 TID:058E013A ERROR: g:\wince700\platform\common\src\soc\mx6q_fsl_v3\vpu\code\vpu.cpp line 3093: PID:00400003 TID:058E013A The EncOpenParam is invalid!

VPU_EncOpen function returns RETCODE_INVALID_PARAM.

Testing was done with a raw YUV file, and had verified all the encoder configuration parameters to be given for VPU_EncOpen.

I am able to test the similar Decoder Application which is displaying the video after decoding a H264/MP4 encoded file.

Please let me know whether anybody has successfully tested the encoder functionality of VPU component with the test application provided.

Thanks in advance.

Regards,

Ashfaque

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

934 Views
skandaprasadp
Contributor I

Hi Ashfaque,

   Even I am facing the same issue for higher Encode width and  height not for 320 x 240 resolution. 

Error thrown :    vpu_EncOpen failed Error code is 0*e

Input source :    720 x 480 resolution YUV format file

output :640 x 480 resolution H264 format file of bitrate 512

Any idea on this problem.

Thanks in advance.

Skandaprasad P

0 Kudos
Reply