Hi,
According to IMX6SXCEC sect.4.2.1 Power-Up Sequence :
[only] USB_OTG1_VBUS and USB_OTG2_VBUS are not part of the power
supply sequence and may be powered at any time.
Is it OK to leave USB_OTG2_VBUS pin float if I don't use USB OTG2?
Or I should pulldown with 10k ohm resister?
Can anyone help me?
Solved! Go to Solution.
Hi torus1000
yes it is ok to leave USB_OTG2_VBUS pin float if one don't use USB OTG2.
It is described in Table 2-17. Recommended connections for unused analog interfaces
IMX6SXHDG Hardware Development Guide for i.MX 6SoloX
http://www.nxp.com/assets/documents/data/en/user-guides/IMX6SXHDG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi torus1000
yes it is ok to leave USB_OTG2_VBUS pin float if one don't use USB OTG2.
It is described in Table 2-17. Recommended connections for unused analog interfaces
IMX6SXHDG Hardware Development Guide for i.MX 6SoloX
http://www.nxp.com/assets/documents/data/en/user-guides/IMX6SXHDG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------