Uboot with USB TTY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,194件の閲覧回数
bonzo
NXP Employee
NXP Employee

For imx devices...

Is it possible to bring up Uboot and use the USB device connector to act as a virtual serial port?  Or is it always necessary to use the RS232 (then a USB-2-Serial adapter).

I know it's possible to use USB as a virtual COM port once the kernel is running.  But I'd like to be able to do this in Uboot and not have to use a usb-2-serial adapter with my laptop.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,540件の閲覧回数
shaojun_wang
NXP Employee
NXP Employee

USB serial driver is not supported in uboot.

The debug message is sent to the uart port.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,541件の閲覧回数
shaojun_wang
NXP Employee
NXP Employee

USB serial driver is not supported in uboot.

The debug message is sent to the uart port.

0 件の賞賛
返信