Hi,
I have upgraded my u-boot with u-boot-6q-no-padding.bin, i have downloaded this one from freescale website.
Now is my tablet bricked, can not boot or go to recovery mode, the only think i can here is a long vibration when i press the power button.
I have tried to put the original u-boot-no-padding.bin using the folowing command without any success:
sudo dd if=u-boot-no-padding.bin of=/dev/sdb bs=1K seek=1; sync
Can anyone help me with this?
Solved! Go to Solution.
I have fixed it using the following command on the internal sd:
sudo dd if=u-boot.bin of=/dev/sdb bs=512 seek=2 conv=fsync
I have used the u-boot from ampe not the freescale one, i don't know what is the difference between them.
how about this?
sudo dd if=u-boot.bin of=/dev/sdb bs=512 seek=2 conv=fsync
I have fixed it using the following command on the internal sd:
sudo dd if=u-boot.bin of=/dev/sdb bs=512 seek=2 conv=fsync
I have used the u-boot from ampe not the freescale one, i don't know what is the difference between them.
Still not working,
I have disassembled the tablet, i can see that there is SD card inside, not mmc, i will try to backup its content
The partition table is:
sudo partx -l /dev/sdb
# 1: 16384- 32767 ( 16384 sectors, 8 MB)
# 2: 32768- 49151 ( 16384 sectors, 8 MB)
# 3: 49152- 3833855 ( 3784704 sectors, 1937 MB)
# 4: 3833856- 31131647 ( 27297792 sectors, 13976 MB)
# 5: 49153- 1097727 ( 1048575 sectors, 536 MB)
# 6: 1097729- 1622015 ( 524287 sectors, 268 MB)
# 7: 1622017- 3719167 ( 2097151 sectors, 1073 MB)
# 8: 3719169- 3735551 ( 16383 sectors, 8 MB)
# 9: 3735553- 3751935 ( 16383 sectors, 8 MB)
should i do cat u-boot-no-padding.bin > /dev/sdb1
or not?