Hi:
I am using uart3 and uart4 on mx6d platform.But uart3 and uart4 cann't send and receive data all the time!
I already check the definition in board_mx6q_sabresd.h:
MX6Q_PAD_EIM_D24__UART3_TXD,
MX6Q_PAD_EIM_D25__UART3_RXD,
MX6Q_PAD_EIM_D23__UART3_CTS,
MX6Q_PAD_EIM_D31__UART3_RTS,
At the same time ,i found the function register as follows:
imx6q_add_imx_uart(4, NULL);
imx6q_add_imx_uart(3, NULL);
imx6q_add_imx_uart(2, NULL);
imx6q_add_imx_uart(1, NULL);
imx6q_add_imx_uart(0, NULL);
Can anyone help me ,uart3 and uart4 cann't send and receive data.
Hi tang
uart4 is used on sabre auto board, please check uboot/include/configs/mx6qsabreauto.h
uboot-imx.git - Freescale i.MX u-boot Tree
use linux build imx6qsabreauto configuration as in attached Yocto Guide
sect.5.1 Build configurations
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI,
igorpadykov
My kernel is linux3.0.35.
I doubt now whether the definition of multi - functional pin multiplexing is wrong.
Can you check it for me?
#define _MX6Q_PAD_EIM_D25__UART3_RXD \
IOMUX_PAD(0x03CC, 0x00B8, 2, 0x0930, 1, 0)
#define _MX6Q_PAD_EIM_D24__UART3_TXD \
IOMUX_PAD(0x03C8, 0x00B4, 2, 0x0000, 0, 0)