I'm trying to flash bootloader(imx-boot) and image(.wic, created with yocto) to EMMC with UUU tool but stucking after wrote "imx-boot".
UUU and u-boot output: pastebin.com/1BFrTJvQ
also, u-boot config: pastebin.com/snxCVxA1
Hello,
I hope you are doing well.
Could you please share the command that you used on UUU?
You need to flash:
<Your file name>.bin-flash_evk
<Your file name>.wic.zst or <Your file name>.wic
For example, here is the command to flash Linux 6.1 on i.MX8MN EVK:
uuu -b emmc_all imx-boot-imx8mn-lpddr4-evk-sd.bin-flash_evk imx-image-full-imx8mn-lpddr4-evk.wic.zst
Best regards.
Jorge.
Hello,
Your board is on serial download mode? You can confirm it with:
uuu -lsusb
With the board in serial download mode and flashing the files mentioned on the last post should be enough to work correctly.
Did you try with the process on the official Coral Dev Board web page? It is listed on section "2: Flash the board".
Best regards.
Jorge.
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172
Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion
==================================================
1:3 MX8MQ SDP: 0x1FC9 0x012B 0x0001
Also, i tried that process you mentioned. I was able to write successfully.