USB OTG Dual role imx8qm-mek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB OTG Dual role imx8qm-mek

Jump to solution
1,746 Views
amit251291
Contributor IV

We want to understand if imx8qm-mek running with Android 9 auto supports USB OTG Dual role (host/device). Please let us know more information on this. 

Tags (3)
0 Kudos
Reply
1 Solution
1,665 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amit

yes it is supported, one can refer to "dr_mode" in

imx8qm-mek.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

and description of usb drivers in Linux 5.4.3_1.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,666 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amit

yes it is supported, one can refer to "dr_mode" in

imx8qm-mek.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

and description of usb drivers in Linux 5.4.3_1.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,666 Views
amit251291
Contributor IV

Thank you igorpadykov‌ for the information. This is helpful. 

0 Kudos
Reply