Two Questions on Running Qt5 webengine on i.mx6q Linux
The following is running chromium-browser. webgl is ok
But there are two problems under Qt5 webengine:
1. The following is running qt-everywhere-src-5.11.2/qtwebengine/examples/webengine/minimal. webgl is ng
but qt-everywhere-src-5.11.2/qt3d/examples/qt3d/lights 3d is ok.
Hi tom
as described in sect.5.6.6 Chromium Browser attached Yocto Guide:
"The Yocto Project community has chromium-imx recipes..Note that NXP does
not support or test the patches from the community, neither for VPU or GPU support."
In general issue also may be posted on meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------