Hi all
I want to know the time until DRAM_RESET goes high and CKE goes high.
I'm using i.MX6UL and DDR3.
Q1.
User can change the value to set by [5: 0] RST_to_CKE of MMDC_MDOR register.
Am I correct ?
Q2.
I set the value to 0x23 but the measured value is 424ns.
I understand that the time change by the parameter but I can't understand how to calculate.
Could you tell me how to calculate ?
I referred the following thread.
So if I need make case, please tell me.
https://community.nxp.com/message/964952
Ko-hey
Solved! Go to Solution.
Hello,
Customers can modify bit field [5: 0] RST_to_CKE of MMDC_MDOR register.
We recommend customers using a 32 K XTAL that has a short start up time, which ensures
that the MMDC initialization is using the 32 KHz XTAL as a reference, instead of the PVT dependent
inaccurate internal osc.
If internal osc is applied in the case, it may be recommended using the Max value in the MDOR - RST_TO_CKE
to ensure that they always are above the 500us spec.This may result in some processors being delayed a little
longer than necessary, but will meet JEDEC specifications.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Customers can modify bit field [5: 0] RST_to_CKE of MMDC_MDOR register.
We recommend customers using a 32 K XTAL that has a short start up time, which ensures
that the MMDC initialization is using the 32 KHz XTAL as a reference, instead of the PVT dependent
inaccurate internal osc.
If internal osc is applied in the case, it may be recommended using the Max value in the MDOR - RST_TO_CKE
to ensure that they always are above the 500us spec.This may result in some processors being delayed a little
longer than necessary, but will meet JEDEC specifications.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri Muhin
Thank you for reply.
I have another question.
Q1.
According to your answer, there is a case different from register setting value.
The cause is mainly PVT and 32KHz XTAL accuracy.
Am I correct ?
Q2.
> If internal osc is applied in the case, it may be recommended using the Max value in the MDOR - RST_TO_CKE to ensure that they always are above the 500us spec.
How to ensure the spec ?
Ensuring by register ?
Ko-hey
Hello,
1.
Correct, PVT and 32KHz XTAL accuracy influences on the timings.
2.
500us is minimal value, Max value in the MDOR - RST_TO_CKE should provide
greater time value.
Regards,
Yuri.