The register of RST_to_CKE of MMDC_MDOR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The register of RST_to_CKE of MMDC_MDOR

Jump to solution
1,655 Views
ko-hey
Senior Contributor II

Hi all

 

I want to know the time until DRAM_RESET goes high and CKE goes high.

I'm using i.MX6UL and DDR3.

 

Q1.

User can change the value to set by [5: 0] RST_to_CKE of MMDC_MDOR register.

Am I correct ?

 

 

Q2.

I set the value to 0x23 but the measured value is 424ns.

I understand that the time change by the parameter but I can't understand how to calculate.

Could you tell me how to calculate ?

 

 

I referred the following thread.

So if I need make case, please tell me.

https://community.nxp.com/message/964952

 

 

Ko-hey

 

Labels (3)
0 Kudos
Reply
1 Solution
1,435 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Customers can  modify bit field [5: 0] RST_to_CKE of MMDC_MDOR register.  

  We recommend customers using a 32 K  XTAL that has a short start up time, which ensures

that the MMDC initialization is using the 32 KHz XTAL as a reference, instead of the PVT dependent

inaccurate internal osc.

  If internal osc is applied in the case, it may be recommended using the Max value in the MDOR - RST_TO_CKE

to ensure that they always are above the 500us spec.This may result in some processors being delayed a little

longer than necessary, but will meet JEDEC specifications.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,436 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Customers can  modify bit field [5: 0] RST_to_CKE of MMDC_MDOR register.  

  We recommend customers using a 32 K  XTAL that has a short start up time, which ensures

that the MMDC initialization is using the 32 KHz XTAL as a reference, instead of the PVT dependent

inaccurate internal osc.

  If internal osc is applied in the case, it may be recommended using the Max value in the MDOR - RST_TO_CKE

to ensure that they always are above the 500us spec.This may result in some processors being delayed a little

longer than necessary, but will meet JEDEC specifications.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,435 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

Thank you for reply.

I have another question.

Q1.

According to your answer, there is a case different from register setting value.

The cause is mainly PVT and 32KHz XTAL accuracy.

Am I correct ?

Q2.

> If internal osc is applied in the case, it may be recommended using the Max value in the MDOR - RST_TO_CKE to ensure that they always are above the 500us spec.

How to ensure the spec ?

Ensuring by register ?

Ko-hey

0 Kudos
Reply
1,435 Views
Yuri
NXP Employee
NXP Employee

Hello,

 1.

    Correct, PVT and 32KHz XTAL accuracy influences on the timings.

2.

  500us is minimal value,   Max value in the MDOR - RST_TO_CKE should provide 

greater time value. 

Regards,

Yuri.