Hi All.
We used the i.MX6 DualLife in the production, the Power dissipation of processors is large, the surface temperature is more than 70℃, now we wants to reduce the power dissipation:
1.Used the USB module, the data of USB write in DDR without ARM core.
2.The power of VPU and GPU are connectted together, we want to use the VPU without the GPU on.
3.We need to use the below processor inter module: USB, IPU, EMMC, MIP, DDR, and close the others.
Can you help to realize the request?
Hi Chris
nxp has special service for such hardware and software optimizations, Professional Services
NXP Professional Services | NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------