The fec1 and fec2 of Imx8qm are opened at the same time. Only fec1 can work, but fec2 cannot
If fec1 is opened separately, fec1 can work; if fec2 is opened separately, fec2 can work.
The software version is imx-androidauto-12.0.0_1.1.0。
The patch has no effect. The phy connected by fec1 can obtain the IP address, while the phy connected by fec2 cannot obtain the IP address. Set the IP manually, and ping the network prompts that the network is unavailable