Hi community,
I have a question about MMPF0100 datasheet.
Please see Table 138, it shows IO DRV register in address 0x90, but there is no description about this register.
Would you let me know the detail, especially RESETBMCU_DRV?
Actually, I want to judge whether I can use RESETBMCU_DRV bit to control RESTBMCU singnal assert/deassert manually.
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Hello,
Basically, in Extended Page 2, most of these registers are used in TEST mode,
and may be marked as reserved. The RESETBMCU_DRV is just for tweaking internal
MOSFET drive parameters, not for asserting / deasserting ; RESETBMCU can't be controlled
manually.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Basically, in Extended Page 2, most of these registers are used in TEST mode,
and may be marked as reserved. The RESETBMCU_DRV is just for tweaking internal
MOSFET drive parameters, not for asserting / deasserting ; RESETBMCU can't be controlled
manually.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------