The detail fo IO DRV in MMPF0100.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The detail fo IO DRV in MMPF0100.

Jump to solution
842 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about MMPF0100 datasheet.

Please see Table 138, it shows IO DRV register in address 0x90, but there is no description about this register.

Would you let me know the detail, especially RESETBMCU_DRV?

Actually, I want to judge whether I can use RESETBMCU_DRV bit to control RESTBMCU singnal assert/deassert manually.

Best Regards,

Satoshi Shimoda

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
643 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically, in Extended Page 2, most of these registers are used in TEST mode,
and may be marked as reserved. The RESETBMCU_DRV is just for tweaking internal

MOSFET drive parameters, not for asserting / deasserting ; RESETBMCU can't be controlled

manually.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
644 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically, in Extended Page 2, most of these registers are used in TEST mode,
and may be marked as reserved. The RESETBMCU_DRV is just for tweaking internal

MOSFET drive parameters, not for asserting / deasserting ; RESETBMCU can't be controlled

manually.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply