The condition to enter i.MX6SDL Wakeup From Low Power Mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The condition to enter i.MX6SDL Wakeup From Low Power Mode.

ソリューションへジャンプ
816件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL boot.

Please see Figure 8-1 in IMX6SDLRM, I want to know the condition to enter "Wakeup From Low Power Mode".

Would you let me know it?

Best Regards,

Satoshi Shimoda

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
731件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

condition : if PGC_CPU_SR=1, then enter "Wakeup From Low Power Mode".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
732件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

condition : if PGC_CPU_SR=1, then enter "Wakeup From Low Power Mode".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信