TLV320AIC3105 on i.MX6Q: no clock on BLCK, WCLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TLV320AIC3105 on i.MX6Q: no clock on BLCK, WCLK

3,253 Views
nguyenmr
Contributor III

I use TI Audio Codec TLV320AIC3105 on our custom boards (iMX6Q, kernel 4.1.15, android 6.0.1). 

I tried to use the  /sound/soc/codecs/tlv320aic3x.c  codec and the /sound/soc/fsl/imx-tlv320aic3x.c machine driver.

In the DTS file, the codec was configured to be compatible with ti,tlv320aic3x. We using gpio to control power supply and reset pin.

In fuction "aic3x_i2c_probe" tlv320aic3x.c, i try to add code read/write some registers of TLV320AIC3105 ic, and show some information. When booting, i see messages show:

tlv320aic3x-codec 2-0018: AIC3x model: 0

tlv320aic3x-codec 2-0018: ai3x-micbias-vg: 2

tlv320aic3x-codec 2-0018: Register 0: 0x 0

tlv320aic3x-codec 2-0018: Register 15: 0x80
tlv320aic3x-codec 2-0018: Register 17: 0xff
tlv320aic3x-codec 2-0018: Register 19: 0x78
tlv320aic3x-codec 2-0018: Register 27: 0xfe

fsl-asrc 2034000.asrc: driver registered

imx-tlv320aic3x sound: data->codec_clk: 24000000

imx-tlv320aic3x sound: tlv320aic3x-hifi <-> 202c000.ssi mapping ok

....

ALSA device list:
 #0: tlv320-audio

 

That's mean I2C interface is OK, and machine driver is mapping ok.

 

But when i try to play music file, i use oscilloscope to check clock on MCLK, BLCK, WCLK, CODEC_DIN and  see that only have clock on MCLK, no clock on BLCK, WCLK, DIN pin.

 

My schematic: 

AUD3_TXFS - WCLK

AUD3_TCX - BLK

AUD3_TXD - CODEC_DIN

AUD3_RDX - CODEC_DOUT

MX6QDL_PAD_GPIO_0__CCM_CLKO1 -> CODEC_MCLK

 

in device tree:

 

pinctrl_i2c3: i2c3grp {
fsl,pins = <
   MX6QDL_PAD_GPIO_3__I2C3_SCL 0x4001b8b1
   MX6QDL_PAD_GPIO_6__I2C3_SDA 0x4001b8b1

 

   /* Audio Codec RESET pin */
   MX6QDL_PAD_GPIO_2__GPIO1_IO02 0x0001b0b0

   >;
};

 

reg_audio: regulator@2 {
   compatible = "regulator-fixed";
   reg = <2>;
   regulator-name = "tlv320aic3105-supply";
   gpio = <&gpio4 10 0>; /* control power supply for audio codec */
   enable-active-high;
};

 

&i2c3 {
   clock-frequency = <100000>;
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_i2c3>;
   status = "okay";


   codec_tlv320: tlv320aic3x@18 {
   compatible = "ti,tlv320aic3x";
   reg = <0x18>;
   clocks = <&clks IMX6QDL_CLK_CKO>;
   ai3x-micbias-vg = <2>;
   gpio-reset = <&gpio1 2 GPIO_ACTIVE_LOW>;
   status = "okay";

   /* Regulators */
   AVDD-supply = <&reg_audio>;
   IOVDD-supply = <&reg_audio>;
   DVDD-supply = <&reg_audio>;
   DRVDD-supply = <&reg_audio>;
};
};

 

sound {
   compatible = "fsl,imx-audio-tlv320aic3x"; 
   model = "tlv320-audio"; 
   cpu-dai = <&ssi2>;
   audio-codec = <&codec_tlv320>;
   ssi-controller = <&ssi2>;

   /* routing of sink, source */
   audio-routing =
      "LINE1L", "Mic Jack",
      "Headphone Jack", "HPLOUT",
      "Headphone Jack", "HPROUT",
      "Ext Spk", "LLOUT",
      "Ext Spk", "LROUT",
      "Mic Jack", "Mic Bias";

   mux-int-port = <2>; 
   mux-ext-port = <3>; 
};

 

&ssi2 {
   fsl,mode = "i2s-master";
   status = "okay";
};

 

pinctrl_audmux: audmuxgrp {
fsl,pins = <
   MX6QDL_PAD_CSI0_DAT7__AUD3_RXD 0x130b0
   MX6QDL_PAD_CSI0_DAT4__AUD3_TXC 0x130b0
   MX6QDL_PAD_CSI0_DAT5__AUD3_TXD 0x110b0
   MX6QDL_PAD_CSI0_DAT6__AUD3_TXFS 0x130b0
   MX6QDL_PAD_GPIO_0__CCM_CLKO1 0x130b0       /* Audio codec clock */
>;
};

 

/* Audio for TLV320AIC3105 */
&audmux {
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_audmux>;
   status = "okay";
};

 

My machine driver and my codec driver is attached.

Anyone has experience onTLV320 can help me?

 

BR/Nguyen

Original Attachment has been moved to: tlv320aic3x.h.zip

Original Attachment has been moved to: tlv320aic3x.c.zip

Original Attachment has been moved to: imx-tlv320aic3x.c.zip

Labels (4)
0 Kudos
Reply
4 Replies

2,040 Views
inkwaterman
Contributor II

Hi Nguen...

I'm facing the same problem ... did you resolved it ?

Can you give tell me how  ?

Many thanks

0 Kudos
Reply

2,040 Views
nguyenmr
Contributor III

Hi,

I searched and try many sources but not successfull. I cannot make SSI give clock out on BLCK, WCLK and Data out.

Now i'm really stuck!

0 Kudos
Reply

2,040 Views
nguyenmr
Contributor III

Today, i can make SSI give clock out on BLCK, WCLK and DOUT when i play music on android app. But i check some audio output pins (RIGHT_LOM, RIGHT_LOP, LEFT_LOM, LEFT_LOP, HPLOUT, HPROUT...) of IC TLV320AIC3105 then no anyone has clock, and of cause, has no sound!

In device tree, i use audio-routing:

"Ext Spk", "LLOUT",

"Ext Spk", "RLOUT",

"Headphone Jack", "HPLOUT",

"Headphone Jack", "HPROUT";

I don't know what's wrong!

BR

0 Kudos
Reply

2,040 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nguen

may be useful to check

How to enable TLV320 on IMX6Q? 

for dts and clocks settings one can look at sabrelite sgtl5000 configuration:

linux-imx6/imx6qdl-sabrelite.dtsi at boundary-imx_4.1.15_1.0.0_ga · boundarydevices/linux-imx6 · Git... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply