TLV320AIC3104-Q1: Need to understand the dynamic switching between two different codec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TLV320AIC3104-Q1: Need to understand the dynamic switching between two different codec

903件の閲覧回数
divyeshmarne0
Contributor III

Hi Team,

Need your help to understand the dynamic switching between two different codec.

We are using:

  1. TLV320AIC3110 - Internal Audio Codec - 0.8W
  2. TLV320AIC3104-Q1 -External Audio Codec (20W*2 Speakers)

So basically we are confused between switching in two codec.

Both the codecs having their own significance.

Could you please suggest any idea to switch between the codecs dynamically.

For example:

if I'm connecting my mobile to Android Device which is having Audio codec thru BT, and I want to play audio from  TLV320AIC3104 External Audio Codec, then what need to be done?

 

thanks.

Divyesh

0 件の賞賛
返信
2 返答(返信)

889件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

818件の閲覧回数
divyeshmarne0
Contributor III

This link is for driver porting. Not helpful.

0 件の賞賛
返信