TLV320AIC3104-Q1: Need to understand the dynamic switching between two different codec

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TLV320AIC3104-Q1: Need to understand the dynamic switching between two different codec

830 次查看
divyeshmarne0
Contributor III

Hi Team,

Need your help to understand the dynamic switching between two different codec.

We are using:

  1. TLV320AIC3110 - Internal Audio Codec - 0.8W
  2. TLV320AIC3104-Q1 -External Audio Codec (20W*2 Speakers)

So basically we are confused between switching in two codec.

Both the codecs having their own significance.

Could you please suggest any idea to switch between the codecs dynamically.

For example:

if I'm connecting my mobile to Android Device which is having Audio codec thru BT, and I want to play audio from  TLV320AIC3104 External Audio Codec, then what need to be done?

 

thanks.

Divyesh

0 项奖励
回复
2 回复数

816 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

745 次查看
divyeshmarne0
Contributor III

This link is for driver porting. Not helpful.

0 项奖励
回复