hello, everyone,
in i.MX8x/i.MX8 MEK, we found that the TCML is the CM4 code bus and the default size is 128K. the TCMU is the system bus and the default size is also 128K.
but the address range is continuous, can we rearrange the default size for data segment and code segment, for example, the data segment size is 128K + 32K, the code segment size is 128K - 32K and vice versa ? if possible, can you help us to prepare a demo and provide us the source code ?
Hi zhao
>can we rearrange the default size for data segment and code segment, for example,
>the data segment size is 128K + 32K, the code segment size is 128K - 32K and vice versa ?
yes
>if possible, can you help us to prepare a demo and provide us the source code ?
this can be done using extended support with Commercial Support and Engineering Services | NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------