Suggest Evaluation Board for IMX50

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suggest Evaluation Board for IMX50

Jump to solution
884 Views
lyfsci
Contributor III

Hi Experts,

Kindly suggest Evaluation Board to quickly start with IMX50 based processors. Also it will be great if it contains all Linux SDK support.

Labels (1)
0 Kudos
Reply
1 Solution
787 Views
SergioSolis
NXP Employee
NXP Employee

Hello Lyf,

Let me suggest the Freescale i.MX50 evaluation board:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX50EVK

You can download the Linux BSP and it is fully supported by Freescale.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
788 Views
SergioSolis
NXP Employee
NXP Employee

Hello Lyf,

Let me suggest the Freescale i.MX50 evaluation board:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX50EVK

You can download the Linux BSP and it is fully supported by Freescale.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply