I have a custom board with iMX6DL and Linux 3.14.28.
The board was idle (only serial console working) -- and suddenly I received a thermal warning..
Touching the iMX6DL -- it was running very cold (no way it was 175 degrees!)
Any idea why this would happen?
Sincerely,
Erez.
Dump on the console:
System is too hot. GPU3D will work at 1/64 clock.
thermal thermal_zone0: critical temperature reached(175 C),shutting down
Broadcast message from root@imx6qsabresd (Sun Jun 21 16:41:56 2015):
The system is going down for system halt NOW!
INIT: Sending processes the TERM signal
logout
▒▒▒▒▒▒▒▒@▒▒▒ނ▒▒@▒▒▒▒▒▒`▒▒▒▒▒@▒▒▒▒▒▒: ▒▒▒▒▒▒▒▒▒▒▒`_▒▒▒O▒▒▒▒O▒▒▒▒`h▒▒▒`3vqi
N
`j`▒▒▒▒▒▒▒▒ ▒▒▒▒▒@▒Ď▒_▒▒▒M▒D ▒▒ŧ▒▒▒▒▒@▒▒ ▒▒▒@▒▒▒.`▒▒▒c▒@▒▒▒▒@▒▒▒▒@▒▒@1onl@▒▒▒▒▒^
▒▒▒z`▒▒▒h▒]▒▒e▒▒n
...done.
Stopping advanced power ▒anagement daemon: no /usr/sbin/apmd found; none killed
apmd.
Stopping system message bus: dbus.
Boot splashscreen disabled
Stopping syslogd/klogd: stopped syslogd (pid 375)
stopped klogd (pid 378)
done
Stopping Telephony daemon
ALSA: Storing mixer settings...
Stopping rpcbind daemon...
done.
Stopping Linux NFC daemon
Deconfiguring network interfaces... ifdown: interface eth0 not configured
done.
Sending all processes the TERM signal...
Hot alarm is canceled. GPU3D clock will return to 64/64
System is too ▒o▒. GP▒3D will work at 1/64 clock.
th▒rma▒ thermal_zone0: critical temperature reached(270 C),shutting down
Please forward me schematic (via Yan).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------