Hi,
I have custom camera connected to IMX6 dual lite processor through LVDS deserializer (THC63LVD1024).
LVDS deserializer (THC63LVD1024) is running in dual-in single out mode.
I have tried different configuration gathered from different threads available on freescale community but none of them worked out for me.
below are settings for getting 16 bit generic data:
IPU_CSI0_SENS_CONF register ==> 0x0400CB00
below are setting for UYVY:
IPU_CSI0_SENS_CONF register ==> 0x0400CA00
Please provide setting to configure 16-bit camera for UYVY format.
If there is some patch available than kindly let me know.
Regards,
Paritosh Singh
How to Support RGB565 Gated Mode Input to i.MX6 CSI
this thread is for rgb565 gate mode, hope helpful for you.