Sporadic iMX6DL Thermal shutdown

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sporadic iMX6DL Thermal shutdown

817 Views
erezsteinberg
Contributor IV

I have a custom board with iMX6DL and Linux 3.14.28.

The board was idle (only serial console working) -- and suddenly I received a thermal warning..

Touching the iMX6DL -- it was running very cold (no way it was 175 degrees!)

Any idea why this would happen?

Sincerely,

Erez.

Dump on the console:

System is too hot. GPU3D will work at 1/64 clock.

thermal thermal_zone0: critical temperature reached(175 C),shutting down

Broadcast message from root@imx6qsabresd (Sun Jun 21 16:41:56 2015):

The system is going down for system halt NOW!

INIT: Sending processes the TERM signal

logout

▒▒▒▒▒▒▒▒@▒▒▒ނ▒▒@▒▒▒▒▒▒`▒▒▒▒▒@▒▒▒▒▒▒: ▒▒▒▒▒▒▒▒▒▒▒`_▒▒▒O▒▒▒▒O▒▒▒▒`h▒▒▒`3vqi

N

`j`▒▒▒▒▒▒▒▒ ▒▒▒▒▒@▒Ď▒_▒▒▒M▒D ▒▒ŧ▒▒▒▒▒@▒▒ ▒▒▒@▒▒▒.`▒▒▒c▒@▒▒▒▒@▒▒▒▒@▒▒@1onl@▒▒▒▒▒^

▒▒▒z`▒▒▒h▒]▒▒e▒▒n

   ...done.

Stopping advanced power ▒anagement daemon: no /usr/sbin/apmd found; none killed

apmd.

Stopping system message bus: dbus.

Boot splashscreen disabled

Stopping syslogd/klogd: stopped syslogd (pid 375)

stopped klogd (pid 378)

done

Stopping Telephony daemon

ALSA: Storing mixer settings...

Stopping rpcbind daemon...

done.

Stopping Linux NFC daemon

Deconfiguring network interfaces... ifdown: interface eth0 not configured

done.

Sending all processes the TERM signal...

Hot alarm is canceled. GPU3D clock will return to 64/64

System is too ▒o▒. GP▒3D will work at 1/64 clock.

th▒rma▒ thermal_zone0: critical temperature reached(270 C),shutting down

Labels (2)
0 Kudos
Reply
1 Reply

462 Views
Yuri
NXP Employee
NXP Employee

  Please forward me schematic (via Yan).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply