Specific HDMI screen resolution 800x480 with i.MX8M-Plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Specific HDMI screen resolution 800x480 with i.MX8M-Plus

ソリューションへジャンプ
586件の閲覧回数
JoelWTK
Contributor II

Hello

I'm working with iot-gate-imx8plus from compulab which integrate i.MX8M-Plus CPU and I have difficulties to use a specific screen with resolution 800x480 over HDMI interface.

From the reference manual of the processor, I have read the following:

HDMI 2.0a Tx supporting one display

Resolutions of: 740x480p60, 720x480p60, 1280x720p60, 1920x1080p60, 1920x1080p120, 3840x2160p30

So the resolution I want is not listed. Is it possible to achieve such resolution ?

I started working on the topic by setting a custom edid file, playing with video= kernel parameter to force 800x480 resolution, but still not working. The best I succeed to do is to have HDMI connected and weston complaining because the the HDMI interface has no modes available

Thanks for feedbacks about this topic (I see it has been discussed many times but no clear answer is done).

Joel

0 件の賞賛
返信
1 解決策
442件の閲覧回数
JoelWTK
Contributor II
0 件の賞賛
返信
4 返答(返信)
443件の閲覧回数
JoelWTK
Contributor II

Hello,

Problem was HDMY PHY clock values available in linux-imx. See https://community.nxp.com/t5/i-MX-Processors/Specific-HDMI-screen-resolution-quot-hdmi-phy-quot-cloc....

Joel

0 件の賞賛
返信
558件の閲覧回数
JoelWTK
Contributor II

Hello @Bio_TICFSL 

Thanks for the reply. Do you know a tutorial somewhere for that ? Looks not so trivial probably ?

Joel

0 件の賞賛
返信
557件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Sorry no, the only information about the hdmi driver is on the Linux reference manual

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

Regards

0 件の賞賛
返信
561件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The resolution is not supported by the driver, in this case you will have to add it and add it to your dtb.

Regards

0 件の賞賛
返信