Specific HDMI screen resolution 800x480 with i.MX8M-Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Specific HDMI screen resolution 800x480 with i.MX8M-Plus

Jump to solution
478 Views
JoelWTK
Contributor II

Hello

I'm working with iot-gate-imx8plus from compulab which integrate i.MX8M-Plus CPU and I have difficulties to use a specific screen with resolution 800x480 over HDMI interface.

From the reference manual of the processor, I have read the following:

HDMI 2.0a Tx supporting one display

Resolutions of: 740x480p60, 720x480p60, 1280x720p60, 1920x1080p60, 1920x1080p120, 3840x2160p30

So the resolution I want is not listed. Is it possible to achieve such resolution ?

I started working on the topic by setting a custom edid file, playing with video= kernel parameter to force 800x480 resolution, but still not working. The best I succeed to do is to have HDMI connected and weston complaining because the the HDMI interface has no modes available

Thanks for feedbacks about this topic (I see it has been discussed many times but no clear answer is done).

Joel

0 Kudos
Reply
1 Solution
334 Views
JoelWTK
Contributor II
0 Kudos
Reply
4 Replies
335 Views
JoelWTK
Contributor II

Hello,

Problem was HDMY PHY clock values available in linux-imx. See https://community.nxp.com/t5/i-MX-Processors/Specific-HDMI-screen-resolution-quot-hdmi-phy-quot-cloc....

Joel

0 Kudos
Reply
450 Views
JoelWTK
Contributor II

Hello @Bio_TICFSL 

Thanks for the reply. Do you know a tutorial somewhere for that ? Looks not so trivial probably ?

Joel

0 Kudos
Reply
449 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Sorry no, the only information about the hdmi driver is on the Linux reference manual

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

Regards

0 Kudos
Reply
453 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The resolution is not supported by the driver, in this case you will have to add it and add it to your dtb.

Regards

0 Kudos
Reply