Hello Team,
I have sabrelite-sd board. I want to create uboot-image, linux-kernel-image for this and boot via SD card.
I have 64-bit machine, with 32-bit ubuntu OS in it.
Please help me with details on -
1. Recommended toolchain for 32-bit ubuntu OS
2. Uboot source code
3. Kernel source code
4. Compilation procedure
5. SD card preparation procedure
Thank you in advance
Supriya
Hi Supriya,
Gary has given you the details reply, it's what you need. Please have a check.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Supriya,
Here are some answers:
1. Recommended toolchain for 32-bit ubuntu OS
$ sudo apt-get install gcc-arm-linux-gnueabihf
2. Uboot source code
Use the nitrogen6q_defconfig since both Nitrogen6x and SabreLite share the same config (as very close).
3. Kernel source code
Use boundary_defconfig, this will build the imx6q-sabrelite.dtb device tree.
4. Compilation procedure
https://boundarydevices.com/compiling-latest-u-boot-for-i-mx6-2015-edition/
https://boundarydevices.com/cross-compiling-kernels-2014-edition-2/
https://boundarydevices.com/ubuntunizing-i-mx6-kernels/
5. SD card preparation procedure
https://boundarydevices.com/ubuntu-trusty-for-i-mx6-boards-february-2016-kernel-3-14-28/
Hope this helps.
Regards,
Gary
Hi Supriya,
If you flash our Trusty image to an SD card, everything will be ready to do for a SabreLite board. You shouldn't even have to compile the kernel or u-boot unless you want to customize them.
BTW I didn't notice your board name but SabreLiteSD doesn't exist, it is either SabreSD or SabreLite.
Regards,
Gary
Hello Gary,
Thanks again for your reply. It is SabreSD board.
For environmental sert-up it is not needed, so I can use pre-built images.
But am trying for the secure booting, where in secure configuration related macro needs to be modified to enable secure booting, hence am trying to build and flash it in sd card.
When I used u-boot.imx and prepared sd card, it was booting up with freescale logo on LCD screen
When I used u-boot.bin and prepared sd card, I was not able to see anything on LCD screen and serial console as well.
dd if=u-boot.bin of=/dev/sdc bs=512 seek=2 conv=fsync
Above is the command I use to prepare the sd card. Please confirm, which binary should I use?
-Supriya
Hi Supriya,
If it's SabreSD, please modify the title of the post (if possible). Also forget all my answers, they only apply to SabreLite, not SabreSD.
Regards,
Gary
Hi Supriya,
About the i.mx6 software and tool you can refer to
i.MX 6 Series Software and Development Tool|NXP
And the board SabreSD board all information you can see as follow:
SABRE for Smart Devices Reference Design|NXP
Hope this can help you.
Any questions you can contact us easily.
Have a great day,
(Dan)
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Dan,
Thank you for your reply. I have run through the links you have provided, which leads to so many other links and documents.
Could you please provide me with specific links on boot source code, linux kernel, rfs, toolchain for SabreSD board?
-Supriya
Under the Solou can see the follow information, here you can see many version of BSP and you can choose one version you need:
And under the Hardware Development Tools you can see the download tool mfgtool in the Programmers link:
And in the documents link you can see the documents to match all the version BSP, you can refer to the use guide document. There are details on how to build the platform and build the BSP and how to run them on your board.
Hope this can help you. If any questions contact me easily.
Have a nice day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------