SECURE BOOT FOR IMX6SX USING TPM CHIP(SE050B)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SECURE BOOT FOR IMX6SX USING TPM CHIP(SE050B)

1,412 Views
ramakrishnathum
Contributor II

We are using imx6sx processor , dunfell branch ,linux 5.4

1.How to use TPM for storing the secure boot keys? Is there any reference for this integration?

2.Is there are specific secure boot document for imx6sx implementation?

Labels (2)
2 Replies

1,194 Views
kanimozhi_t
Contributor V

@ramakrishnathum @Rita_Wang We're interested in a similar approach. If you have any updates or leads that would be highly appreciable.

0 Kudos
Reply

1,356 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

All the documents for i.MX6SX are here i.MX 6SoloX Applications Processors | Arm® Cortex®-A9, Cortex-M4 | NXP .

https://www.nxp.com/docs/en/application-note/AN12056.pdf

one can refer to the Reference Manual, which has brief introduction.

0 Kudos
Reply