refer to the bsp code, it seems
the bit24 is Standard tuning circuit and procedure enable
This field is used to enable standard tuning circuit and procedure.
bit 16-18:TUNING_STEP
The increasing delay cell steps in tuning procedure
bit 7:
Disable command check for standard tuning
Writing 1 to this field disables command check (command CRC, CMD end bit error, and CMD index error
or CMD timeout error) for standard tuning flow after each tuning command is sent
bit0-6:
Tuning start
The start delay cell point when send first CMD19 in tuning procedure