SD card image of IMXEBOOKDC3-E (E-ink panel)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SD card image of IMXEBOOKDC3-E (E-ink panel)

跳至解决方案
1,035 次查看
torus1000
Contributor V

Hi,

I accidentally crashed my bundled SD card which attached to the IMXEBOOKDC3-E (E-ink panel for MX6SL-EVK) and I don't have any backup of it.

Where can I download the SD card image labeled "MX6SLEVK-E-INK ANDROID r12.10.02"?

Is it exactly same demo image as KK442* or L500** except bootargs*** ?

where

  * KK442: https://www.nxp.com/webapp/Download?colCode=KK442_100_ANDROID_DEMO_EVK_BSP

  ** L500: https://www.nxp.com/webapp/Download?colCode=IMX6-L500-100-DEMO-EVK-BSP

  *** bootargs: video=mxcepdcfb:E060SCM,bpp=16 max17135:pass=2,vcom=-2030000

Can anybody help me?

BR

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
743 次查看
b36401
NXP Employee
NXP Employee

I placed my Android SD card image for iMX6SL EVK with E-INK here:

http://photo.afti.ru/tmp/fs/imx6sl-evk-eink-android.image.gz

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
744 次查看
b36401
NXP Employee
NXP Employee

I placed my Android SD card image for iMX6SL EVK with E-INK here:

http://photo.afti.ru/tmp/fs/imx6sl-evk-eink-android.image.gz

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
743 次查看
torus1000
Contributor V

I found following thread.

Kitkat support for EPD in i.mx6slevk

https://freescale.jiveon.com/thread/334197

The latest Android BSP that supported the i.MX6SL EPD is Android Ice Cream Sandwich (R13.5).

So I will try this later.

Demo Image Flashed on the i.MX 6SoloLite EVK SD Cards (REV R13.5)  ZIP  (1.6 GB) 11/9/2012

https://www.nxp.com/webapp/Download?colCode=IMX6_SL_SDP_SD_DEMO_IMAGE

0 项奖励
回复