Is the Reset_b signal on i.MX25 level-sensitive or edge-sensitive?
I am currently working on a prototype board with i.MX258, and found that the processor keeps running when Reset_b input is asserted low. Untile Reset_b returns high, the processor restarts.
It seems it's a positive edge-triggered singal, only the rising edge leads to a reset event. But it's not clearly stated in the manual, so I want to make sure is it the expected behaviour?
What's the reset timing like?
已解决! 转到解答。
Yes, you are right. The RESET_B input of the i.MX25 processor is edge-sensitive. The reset logic operates as follows: first, it detects a rising edge of the RESET_B signal, then it qualifies that RESET_B remains high during 4 CKIL cycles, and after that the cold reset occurs.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, you are right. The RESET_B input of the i.MX25 processor is edge-sensitive. The reset logic operates as follows: first, it detects a rising edge of the RESET_B signal, then it qualifies that RESET_B remains high during 4 CKIL cycles, and after that the cold reset occurs.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------